Hi,
After following the installation process and running the installation file as an admin, I get the following error when trying to open PSpice.
It seems there is a problem communication with the Liscense server...
One interesting thing to note is that when I finish the installation process and select the option to open PSpice after installation, it runs just fine. I close it and try to open it again and the above error message is displayed.
Is this something you can help me with?
BR,
Vemund Dybvik