When troubleshooting problems with PSpice for TI or TI-developed PSpice models, we may need certain log files. The file locations are often determined by Microsoft Windows environment variables such as "HOME" and "APPDATA". These are actual Windows directories.
An example of the log files often needed is "cdsPspiceTIlog.txt" which is in the directory "%appdata%\Cadence\PSpiceTIInstall".
(Typically C:\Users\ < your username > \AppData\Roaming\Cadence\PSpiceTIInstall\cdsPspiceTIlog.txt )
The easiest way to get there is to copy and paste the path into Windows Explorer.
Now press "Enter". Windows explorer will automatically change to the correct location:
Please collect this log file and please click here to open a new thread on the PSpice for TI E2E forum.