This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PSpice-for-TI: Unable to make index for library file 'nom_pspti.lib'

I got this error , and I've run 'reinstall TI models and libraries' several times and it still shows the error.

Is there any other solution?

 

error log:

0.3.
**** 03/17/22 09:55:02 ******* PSpice 17.4.0 (Nov 2018) ******* ID# 0 ********

** Profile: "SCHEMATIC1-bias" [ c:\users\redding\desktop\test\test-pspicefiles\schematic1\bias.sim ]


**** CIRCUIT DESCRIPTION


******************************************************************************


** Creating circuit file "bias.cir"
** WARNING: THIS AUTOMATICALLY GENERATED FILE MAY BE OVERWRITTEN BY SUBSEQUENT SIMULATIONS

*Libraries:
* Profile Libraries :
* Local Libraries :
* From [PSPICE NETLIST] section of C:\cds_spb_home\cdssetup\OrCAD_PSpiceTIPSpice_Install\17.4.0\PSpice.ini file:
.lib "nom_pspti.lib"
.lib "nom.lib"

*Analysis directives:
.TRAN 0 1ms 0
.OPTIONS ADVCONV
.OPTIONS FILEMODELSEARCH
.PROBE64 V(alias(*)) I(alias(*)) W(alias(*)) D(alias(*)) NOISE(alias(*))
.INC "..\SCHEMATIC1.net"

**** INCLUDING SCHEMATIC1.net ****
* source TEST
C_C1 0 N14382 1n TC=0,0
R_R1 N14375 N14382 1k TC=0,0
V_V1 N14375 0 DC 0Vdc AC 1Vac

**** RESUMING bias.cir ****
.END

WARNING(ORPSIM-15246): Library index file nom_pspti.ind does not have the correct format

INFO(ORPSIM-15422): Making new index file nom_pspti.ind for library file nom_pspti.lib.

.lib "tps6c5912_trans.lib"

ERROR(ORPSIM-15116): Unable to find library file tps6c5912_trans.lib.

Index has 78904 entries from 3851 file(s).

ERROR(ORPSIM-15107): Unable to make index for library file C:\cds_spb_home\cdssetup\pspTILibDir\nom_pspti.lib.