Part Number: TIDM-02007
Hi Team,
My customer is currently debugging based on TIDM-02007. At present, when testing Level 4, it is found that the motor cannot start normally (it shows that the motor does not move, but there is current, which is similar to motor stall)
In the current test, if the ABI interface is not inserted, the motor can work in the state of “Wait for index ” and rotate at low speed. This shows that the hardware and software are normal.
This can also happen if the UVW is wired incorrectly during my previous tests. However, after the customer changed the UVW wiring, the motor still does not rotate (but there is current).
Due to the current impact of covid-19, I cannot enter the laboratory for testing experiments, so I seek your support. Do you have any comments on this?
Thanks
Jenson