Other Parts Discussed in Thread: TMS320F280025C,
Hi,
I wanted a clarification regrading ADC
While doing unit testing with TMS320F280025C launch pad, I wanted to see if the counts are correct.
MTR2_IU_ADCRESLT (MTR2_IU_ADCRES_BASE + ADC_O_RESULT9) ------ (1)
For the above code,
ADC_O_RESULT 9 value is 3001
and
MTR2_IU_ADCRES_BASE value is 0x00000B00U whose equivalent decimal is 2816
Therefor,
MTR2_IU_ADCRESLT value = 3001+2816
= 5817
Is this value correct? Can anyone help me on this