Part Number: PMP10344
Hi
I would like to know the purpose of this part of the circuit, in PMP10344:

And how can I shrink the Power Supply size, if possible.
Regards.
Arion
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: PMP10344
Hi
I would like to know the purpose of this part of the circuit, in PMP10344:

And how can I shrink the Power Supply size, if possible.
Regards.
Arion
Hi Arion,
D2, D4 and R1 are the clamp circuit that limits the voltage in the flyback primary MOSFET. This is used to limit the voltage spikes due to the leakage inductance of the transformer.
To reduce the size is a much more difficult question, are there any specifications that are different from this design?
Thanks,
Robert
Hi Robert.
Thank you for the answer.
Can I reduce the size of the varistor, using a SMD for example? Or reduce the size of the 0.01uF/1000V capacitor?
Thanks.
Arion
Hi Arion,
My initial thought is no, but I am looping in the original design to comment.
Thanks,
Robert
Hi Arion,
The varistors are there for surge protection, and do not play role in the actual power conversion. I don't think you will find any varistors that are significantly smaller, but if you already have surge protection elsewhere in your system you could remove them.
I think 0.01uF capacitor could possibly be removed. It is there to help suppress conducted EMI at higher frequencies, but there is plenty of margin above 10MHz.
thanks,
Brian