This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TIDM-02010: Error linking files

Part Number: TIDM-02010

In TIDM-2010 software we are incorporating communication part into our main program, we are facing errors. I have explicated one case of motor 1 voltage variable below.

  • In modbus_slave.c  we have created our communication software. We have all the values of PFC,motor1 and motor2 to transmit for GUI. The code corresponding to motor 1 (compressor motor) is given as per the snippet below.

                                                                        modbus_slave.c

    extern MTR1_VU_VFD;

case 6:

        g_st_Act.u16_M1_VU = MTR1_VU_VFD;

        x = (g_st_Act.u16_M1_VU) * 100;

        break;

  • As the motor voltage values are addressed in hal.h we have taken the variables from modbus_slave and we are trying to call the voltage value from hal.h to GUI. The value that goes to GUI is read as MTR1_VU_VFD. The code snippet for the same is given below as highlighted.

 

                                                                        hal.h

float32_t MTR1_VU_VFD = 0.0;

#if defined(MOTOR1_FAST)

   

    // convert phase A voltage

   

    value = (float32_t)ADC_readResult(MTR1_VU_ADCRES_BASE, MTR1_VU_ADC_SOC_NUM);

    pADCData->V_V.value[0] = value * pADCData->voltage_sf;

 

    MTR1_VU_VFD = pADCData->V_V.value[0]; // to GUI

 After running the project, we are getting such errors.

Description Resource Path Location Type
#10010 errors encountered during linking; "tidm_02010_dmpfc_002x_simple.out" not built tidm_02010_dmpfc_002x C/C++ Problem
#10056 symbol "M1_VU_VFD" redefined: first defined in "./sys_main.obj"; redefined in "./src_board/hal.obj" tidm_02010_dmpfc_002x C/C++ Problem
#10056 symbol "M1_VU_VFD" redefined: first defined in "./sys_main.obj"; redefined in "./src_board/user_mtr1.obj" tidm_02010_dmpfc_002x C/C++ Problem
#10056 symbol "M1_VU_VFD" redefined: first defined in "./sys_main.obj"; redefined in "./src_board/user_mtr2.obj" tidm_02010_dmpfc_002x C/C++ Problem
#10056 symbol "M1_VU_VFD" redefined: first defined in "./sys_main.obj"; redefined in "./src_board/user_pfc.obj" tidm_02010_dmpfc_002x C/C++ Problem
#10056 symbol "M1_VU_VFD" redefined: first defined in "./sys_main.obj"; redefined in "./src_control/motor_common.obj" tidm_02010_dmpfc_002x C/C++ Problem
#10056 symbol "M1_VU_VFD" redefined: first defined in "./sys_main.obj"; redefined in "./src_control/motor1_drive.obj" tidm_02010_dmpfc_002x C/C++ Problem
#10056 symbol "M1_VU_VFD" redefined: first defined in "./sys_main.obj"; redefined in "./src_control/motor2_drive.obj" tidm_02010_dmpfc_002x C/C++ Problem
#10056 symbol "M1_VU_VFD" redefined: first defined in "./sys_main.obj"; redefined in "./src_control/pfc_ctrl.obj" tidm_02010_dmpfc_002x C/C++ Problem

Even though the variable names are changed we are facing these errors.

Can anyone pls help out?