Other Parts Discussed in Thread: BQ76940, BQ34Z100,
Hi,
CAN_T and CAN_R from/to CAN Transceiver are connected to MSP430 P1.0 and p1.1. Should these two pins configured as GPIOs ? Or can they be used as SPI?
On the system, users might want to use CAN bus to issue commands to Bq76940 or BQ34z100. How are CAN_T and CAN_R from CAN BUS communication translated to I2C commands on MSP430? Is there readily available sample code running on MSP430 that can be shared? Thanks,
Eric