Hi Team,
I want to simulate a halfbridge-design with different dead-times in the PWM-Signal.
The PWM-Signal should have a frequency of 20kHz and its duty cycle should vary from 5% to 95% in order to create a sinusoidal wave, when the PWM-Signal is inputted to an inductor.
In addition the PWM-signals of high side and low side switches of the halfbridge should contain a dead-time to prevent a short-through.
How can I create this PWM-Signal? I tried with the voltage generator - general waveform, but here I cant vary the duty cycle over time.
An example of the PWM signal is shown in the image "pwm" and the application in the image "application" below.