Part Number: TIDA-010042
Other Parts Discussed in Thread: LM5109, INA280, INA240, LM5009, LM5168
Hi, I have solar panel with output 15Watt and open circuit voltage 111V. I need to interface with TIDA-010042. TIDA-010042 maximum input voltage is 15 V to 60 V but our solar panel Voc is 111V max.
How to use TIDA-010042 in our application or any other IC suitable for out solar panel which Voc is 111Volt