Other Parts Discussed in Thread: TPS92641
Hi Team,
I have a question that needed clarification for the TIDA-080008 .
In the documentation, Table 2 indicates that the max voltage output is configured for is approx 15.8V, then it is also mentioned up to 31.6V in the top side pump configuration with two LEDs in series on the green channel (www.ti.com/.../tiduew9). The EVM for the TPS92641 also supports up to 33V output (www.ti.com/.../slvu823.pdf
The customer have LEDs that they want to drive have opening voltages in the 16.8-22.4V range - given the headroom on the green channel up to 31.6V with top side pump, I assume the board will support these slightly higher voltages? Is this correct?
I hope you can clarify.
Regards,
Marvin