Other Parts Discussed in Thread: UCC28911, UCC28910, LM5021
Hi team
Customer is looking for the optimized solution with below requirements. Is the design able to support?
Input voltage: AC80-120V
Output voltage: DC 14.5V +/- 0.5V
Load current: min 5mA, max 700mA
SW freq: >100kHz
Best regards,
Hayashi