Part Number: TIDA-010025
Dear Team,
I am working on building an variable output AC supply for testing purposes. Could TIDA-010025 be modified to work as an adjustable output AC source?
Best Regards,
Caglar
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TIDA-010025
Dear Team,
I am working on building an variable output AC supply for testing purposes. Could TIDA-010025 be modified to work as an adjustable output AC source?
Best Regards,
Caglar
Hi Caglar,
good to hear from you!
Thank you for your interest in the TIDA-010025. The TIDA-010025 is a PWM switched 2-level 3-phase AC inverter. We can run it in open loop t generate a 3-phase AC output voltage with variable magnitude and frequency by using an appropriate sinusoidal PWM modulation from e.g. 0Hz to 50Hz and a magnitude scale from 0 to 1, where 1 would
give a peak amplitude of 0.5-times the DC-bus voltage.
The output phase (to DC-) voltage is a PWM modulated output at two levels DC+ and DC- switched at the PWM carrier, e.g. 10kHz. To get an sinusoidal phase to phase voltage
the PWM carrier we need to be remove the PWM carrier with e.g. an appropriate LC filter.
Is that what you were looking for?
Regards,
Martin Staebler
Hi Caglar,
following our discussion with your customer by email directly, I understood that the above explanation was clear enough for your customer the to understand the use case of TiDA-010025 with respect to a variable frequency and magnitude AC output voltage.
Therefore I am closing this case.
Regards, Martin