This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

P spice will not install due to FIPS encryption, but its disabled

I am trying to install Psipce and the FIPS encryption is disabled on my computer, but there is still an error when I try to install it saying that the FIPS needs to be disabled(which it is).  Any ideas?

Thanks

  • this is the install file so far

    [0x0409]
    1100=Setup Initialization Error
    1101=%s
    1102=%1 Setup is preparing the %2, which will guide you through the program setup process. Please wait.
    1103=Checking Operating System Version
    1104=Checking Windows(R) Installer Version
    1105=Configuring Windows Installer
    1106=Configuring %s
    1107=Setup has completed configuring the Windows Installer on your system. The system needs to be restarted in order to continue with the installation. Please click Restart to reboot the system.
    1108=%s
    1125=Choose Setup Language
    1126=Select the language for this installation from the choices below.
    1127=The installer must restart your system to complete configuring the Windows Installer service. Click Yes to restart now or No if you plan to restart later.
    1128=This setup will perform an upgrade of '%s'. Do you want to continue?
    1129=A later version of '%s' is already installed on this machine. The setup cannot continue.
    1130=OK
    1131=Cancel
    1132=Password:
    1133=Install
    1134=&Next >
    1150=Setup has detected an incompatible version of Windows. Please click OK and verify that the target system is running either Windows 95 (or later version), or Windows NT 4.0 Service Pack 6 (or later version), before relaunching the installation
    1151=Error writing to the temporary location
    1152=Error extracting %s to the temporary location
    1153=Error reading setup initialization file
    1154=Installer not found in %s
    1155=File %s not found
    1156=Internal error in Windows Installer
    1158=Error populating strings. Verify that all strings in Setup.ini are valid.
    1200=Restart
    1201=Setup needs %lu KB free disk space in %s. Please free up some space and try again
    1202=You do not have sufficient privileges to complete this installation for all users of the machine. Log on as administrator and then retry this installation
    1203=Command line parameters:
    1204=/L language ID
    1205=/S Hide initialization dialog. For silent mode use: /S /v/qn
    1206=/V parameters to MsiExec.exe
    1207=Windows(R) Installer %s found. This is an older version of the Windows(R) Installer. Click OK to continue.
    1208=ANSI code page for %s is not installed on the system and therefore setup cannot run in the selected language. Run the setup and select another language.
    1210=Setup requires Windows Installer version %s or higher to install the Microsoft .NET Framework version 2.0. Please install the Windows Installer version %s or higher and try again.
    1603=Error installing Windows Installer engine. A file which needs to be replaced may be held in use. Close all applications and try again.
    1604=This setup does not contain the Windows Installer engine (%s) required to run the installation on this operating system.
    1607=Unable to install %s Scripting Runtime.
    1608=Unable to create InstallDriver instance, Return code: %d
    1609=Please specify a location to save the installation package.
    1611=Unable to extract the file %s.
    1612=Extracting files.
    1613=Downloading file %s.
    1614=An error occurred while downloading the file %s. What would you like to do?
    1615=hr
    1616=min
    1617=sec
    1618=MB
    1619=KB
    1620=/sec
    1621=Failed to verify signature of file %s.
    1622=Estimated time remaining:
    1623=%1 %4 of %2 %4 downloaded at %3 %4/sec
    1624=Preparing to Install...
    1625=Get help for this installation.
    1626=Help
    1627=Unable to save file: %s
    1628=Failed to complete installation.
    1629=Invalid command line.
    1630=/UA<url to InstMsiA.exe>
    1631=/UW<url to InstMsiW.exe>
    1632=/UM<url to msi package>
    1633=/US<url to IsScript.msi>
    1634=Setup Initialization Error, failed to clone the process.
    1635=The file %s already exists. Would you like to replace it?
    1642=Could not verify signature. You need Internet Explorer 3.02 or later with Authenticode update.
    1643=Setup requires a newer version of WinInet.dll. You may need to install Internet Explorer 3.02 or later.
    1644=You do not have sufficient privileges to complete this installation. Log on as administrator and then retry this installation
    1645=Error installing Microsoft(R) .NET Framework, Return Code: %d
    1646=%s optionally uses the Microsoft (R) .NET %s Framework. Would you like to install it now?
    1648=Setup has detected an incompatible version of Windows. Please click OK and verify that the target system is running either Windows 95 (or later version), or Windows NT 4.0 Service Pack 3 (or later version), before relaunching the installation
    1649=%s optionally uses the Visual J# Redistributable Package. Would you like to install it now?
    1650= (This will also install the .NET Framework.)
    1651=Setup has detected an incompatible version of Windows. Please click OK and verify that the target system is running Windows 2000 Service Pack 3 (or later version), before relaunching the installation
    1652=%s requires the following items to be installed on your computer. Click Install to begin installing these requirements.
    1653=Installing %s
    1654=Would you like to cancel the setup after %s has finished installing?
    1655=The files for installation requirement %s could not be found. The installation will now stop. This is probably due to a failed, or canceled download.
    1656=The installation of %s appears to have failed. Do you want to continue the installation?
    1657=Succeeded
    1658=Installing
    1659=Pending
    1660=Installed
    1661=Status
    1662=Requirement
    1663=Failed
    1664=Extracting
    1665=Downloading
    1666=Skipped
    1667=The installation of %s has failed. Setup will now exit.
    1668=The installation of %s requires a reboot. Click Yes to restart now or No if you plan to restart later.
    1669=%1 optionally uses %2. Would you like to install it now?
    1670=Unable to load module %s, Error Code: %d
    1671=Downloading file %2 of %3: %1
    1700=An error occurred initializing the InstallScript engine
    1701=Unable to extract InstallScript engine support files to temp location
    1702=This installation lets you install multiple instances of the product. Select the instance you would like to install, and then click Next to continue:
    1703=&Install a new instance
    1704=&Maintain or upgrade an existing instance
    1705=Default
    1706=Instance ID
    1707=Product Name
    1708=Location
    1710=This installation lets you patch multiple instances of the product. Select an option below to specify how you would like to apply this patch, and then click Next to continue.
    1711=Patch &all of the existing instances
    1712=&Patch an existing instance
    1713=This installation requires Windows Installer version 4.5 or newer. Setup will now exit.
    1714=Decompressing
    1715=Version
    1804=Choose Setup Language
    1812=Select the language for the installation from the choices below.
    1813=&OK
    1815=InstallShield Wizard
    1822=Cancel
    1834=&Next >
    1835=< &Back
    1837=Do you wish to install %s?
    1838=Authenticity Verified
    1839=The identity of this software publisher was verified by %s.
    1840=Caution: %s affirms this software is safe. You should only continue if you trust %s to make this assertion.
    1841=&Always trust software published by %s.
    1842=This software has not been altered since publication by %s. To install %s, click OK.
    1854=InstallShield
    1865=Preparing Setup
    1866=Please wait while the InstallShield Wizard prepares the setup.
    1872=Finish
    1873=Transfer rate:
    1874=Estimated time left:
    1880=/s
    1887=%s - InstallShield Wizard
    1888=Exit Setup
    1889=Are you sure you want to cancel the setup?
    1901=&Install a new instance of this application.
    1903=Existing Installed Instances Detected
    1904=Select the appropriate application instance to maintain or update.
    1905=Setup has detected one or more instances of this application already installed on your system.
    1906=&Maintain or update the instance of this application selected below:
    1907=Setup has detected one or more instances of this application already installed on your system. You can maintain or update an existing instance or install a completely new instance.
    1908=Select the instance of the application you want to &maintain or update below:
    1909=Display Name
    1910=Install Location
    2001=%s Setup is preparing the InstallShield Wizard, which will guide you through the rest of the setup process. Please wait.
    2002=Error Code:
    2003=Error Information:
    2004=An error (%s) has occurred while running the setup.
    2005=Please make sure you have finished any previous setup and closed other applications. If the error still occurs, please contact your vendor: %s.
    2006=&Detail
    2007=&Report
    2008=There is not enough space to initialize the setup. Please free up at least %ld KB on your %s drive before you run the setup.
    2009=A user with administrator rights installed this application. You need to have similar privileges to modify or uninstall it.
    2010=Another instance of this setup is already running. Please wait for the other instance to finish and then try again.
    2143=Security Warning
    2144=Do you want to run this setup?
    2146=The origin and integrity of this application could not be verified. You should continue only if you can identify the publisher as someone you trust and are certain this application hasn't been altered since publication.
    2147=I &do not trust this setup
    2148=I &understand the security risk and wish to continue
    2151=The origin and integrity of this application could not be verified because it was not signed by the publisher. You should continue only if you can identify the publisher as someone you trust and are certain this application hasn't been altered since publication.
    2152=The origin and integrity of this application could not be verified. The certificate used to sign the software has expired or is invalid or untrusted. You should continue only if you can identify the publisher as someone you trust and are certain this application hasn't been altered since publication.
    2153=The software is corrupted or has been altered since it was published. You should not continue this setup.
    2154=This setup was created with a BETA VERSION of %s
    2155=This Setup was created with an EVALUATION VERSION of %s
    2156=Please enter the password
    2157=This setup was created with an EVALUATION VERSION of %s, which does not support extraction of the internal MSI file. The full version of InstallShield supports this functionality. For more information, see InstallShield KB article Q200900.
    2158=This setup was created with an EVALUATION VERSION of %s. Evaluation setups work for only %s days after they were built. Please rebuild the setup to run it again. The setup will now exit.
    2159=This setup works until %s. The setup will now exit.

    [Languages]
    0x0401=Arabic
    0x0402=Bulgarian
    0x0403=Catalan
    0x0404=Chinese (Traditional)
    0x0405=Czech
    0x0406=Danish
    0x0407=German
    0x0408=Greek
    0x0409=English (United States)
    0x040a=Spanish
    0x040b=Finnish
    0x040c=French (Standard)
    0x040d=Hebrew
    0x040e=Hungarian
    0x0410=Italian
    0x0411=Japanese
    0x0412=Korean
    0x0413=Dutch
    0x0414=Norwegian
    0x0415=Polish
    0x0416=Portuguese (Brazilian)
    0x0418=Romanian
    0x0419=Russian
    0x041a=Croatian
    0x041b=Slovak
    0x041d=Swedish
    0x041e=Thai
    0x041f=Turkish
    0x0421=Indonesian
    0x0424=Slovenian
    0x042d=Basque
    0x0804=Chinese (Simplified)
    0x0816=Portuguese (Standard)
    0x0c0c=French (Canadian)
    0x0c1a=Serbian (Cyrillic)

  • Hi Patrick,

    Are you using Windows 10 OS?

    Please share the file located at: C:\Users\ < your username > \AppData\Roaming\Cadence\PSpiceTIInstall\cdsPspiceTIlog.txt

    Thank you,

    Jackie