Part Number: TIDA-010057
Other Parts Discussed in Thread: TX7332, , AFE5832LP
Hi Team,
Hope you are well!
My customer, Zimmer Biomet, ran into a strange ramp pattern using our AFE5832LP and the TX7332 in conjunction with TIDA-010057. Please see their details below and let me know if any more information is needed.
Some notes from our investigation:
-observed that output of TX was only going between HVP and 0V. Found that L43 was missing (ferrite bead; connection for HVM from TIDA) – reconnecting HVM led to TIDA overheating and triggering USB port current over-loads.

-disconnecting HVP and HVM, was able to reproduce problematic ramping with TI’s FPGA load and SW, TIDA still overheating.
-disconnecting all the analog supplies to Tx and Rx chips resolved overheating. Keeping 1.2V_DVDD and 1.8V_DVDD connected allowed the Rx chip appears to be able to communicate with the FPGA. The TIDA did not experience excessive heat up, but test patterns could no longer be generated.
-investigation with thermal camera found that Tx chip connected to Rx B was getting hotter than the rest
Thanks!
Connor