This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TIDA-00915: Does TIDA-00915 could be configured to run as full bridge by firmware?

Part Number: TIDA-00915


Does TIDA-00915 could be configured to run as full bridge by firmware?

Thanks!

  • Hi Xiaonan,

    The inverter stage of this reference desing is a three-phase full-bridge inverter, and normally, the controller's firmware should be configured to run it in this mode.

    As for the input, it requires a DC input within the 200V~400V range. If you would like to use an AC input, then external rectifier stage and DC bus capacitor to convert it into a DC voltage are needed. Please make sure the converted DC voltage is with the 200V~400V range.

    Best regards,

    Jerome Shan

  • TIDA-00915: Does TIDA-00915 could be configured to run as full bridge by firmware?

    I did not get a right answer from Jerome!

  • The application note says it is half bridge.

  • Hi Xiaonan,

    For the inverter stage, at the begining of the Design Guide in the Description section, it mentions "this reference design is a three-phase inverter ... for driving 200-V AC servo motors". In Page 9 of the Design Guide, it mentions  "the power stage consist of three identical half bridges", and thus surely it can be configures to run as a three-phase full briage inverter, so as to drive an AC motor.

    For the converter stage, this reference design does not have a high voltage converter stage to rectify an AC power input. It only accepts high voltage DC input of 200V~400V via J5. Please refer to Page 18 of the Design Guide for Figure 17 of the 'Test Connections' and Table 2 of 'Key System Specifications' in Page 3 for the 'DC link voltage' spec.

    Best regards,

    Jerome Shan