Other Parts Discussed in Thread: TPS25750, BQ25792
Hello,
My team and I are designing a portable battery which charges and discharges via USB-C. We would like to know if this design is capable of sourcing 20V/3A from the battery.
The 5V/5A buck is somewhat confusing to me in the diagram. From what I can tell, the 5V/5A buck outputs to power the TPS25750 and the LDOs attached to it. It also can output to the device attached to the battery.
Is the TPS25750 capable to telling the BQ25792 to source 20V/3A to the device?