This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

piecewise linear: how? tina

Other Parts Discussed in Thread: TINA-TI

I am attempting to build the following signal:

Start at t=0, V=0.944

at t=3.23usec, V=1.2V (ramped up)

at t=3.24usec, V=0

repeating at 5usec intervals.

I'm trying this with the piecewise linear model, which I'm getting nowhere with.  I'll add that I have not used pspice in 20 years, so I would expect the help section to explain how to add commands.  If another model could be used instead, please point me in that direction. 

This work is to help the largest customer in New England.

 

jack