This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TIDA-010054: DC blocking capacitor

Part Number: TIDA-010054


Hello,

In dual active bridge topology mentioned in "TIDA-DAB-010054", How to calculate the DC blocking capacitor value.

There are 14 DC blocking capacitors used in parallel to each other in both primary & secondary.

Each winding has value of 14 x 0.47uF = 6.58uF.

How to calculate the value of DC block capacitor in DAB topology?

This is not mentioned in the DAB design guide.

Regards,

Abhishek Deshmukh