This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PMP20859: If I don't require external 48V input, do I just delete the ringed components below ?

Part Number: PMP20859


I require a dual PoE input design, but no external 48V input, so do I just delete the components ringed below. Looks like I won't need the 48V input connector, 48V sense control and 2 off circuits to pull (PoE) PG low if external 48V is present as used on the PMP20859.