Part Number: PMP40871
Other Parts Discussed in Thread: TPS61391
Hi team,
How is the load regulation at >25mA? Customer's phantom power is 28mA as max. And is there any side effect over 20mA?

Best regards,
Hayashi
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Hayashi,
Sorry for the slow response. If the input voltage is 3.3V, the TPS61391 will not be able to supply 48V output at 28mA, because it will be limited by the peak current limit and DCM operation (see section 8.2.2.2 of the TPS61391 data sheet.) If the input voltage is 5V, you can use a 5.6uH inductor to keep the peak inductor current below the 800mA limit and remain in DCM with a 48V/28mA output.
thanks,
Brian
Hi Brian,
I understand there is limitation when input voltage is 3.3V. But when I look the attached figure, there are voltage drop above 22.5mA. Will these be linear decrease above 25mA?
Regards,
Hayashi
Hi Hayashi,
It won't really be linear, but the output voltage will continue to decrease. It will behave more like a constant power limit, since the input current is limited by the peak current limit and the input voltage is fixed.
thanks,
Brian