Other Parts Discussed in Thread: TIDA-01604, TIDA-01605
Hi Team,
Why in TIDA-01604 is preferred to use TIDA-01605 instead of TIDA-010054?
in TIDA-010054, there is the part "Short circuit Detection & Two Level Turn Off For high side switch". in TIDA-01605, the part "Short circuit Detection & Two Level Turn Off For high side switch" is not there. Beyond the pin that doesn't match, I was wondering why this part is not included in TIDA-01605, is it useless for that type of application?
Best Regards,
James