Part Number: TIDA-00443
Hi,
In section 4.2.4, the VF_bridge per element is taken as 0.85 V for loss calculation. Could you please let me know from where this information is obtained. In the datasheet of GBJ1508, it is only mentioned that VF_bridge per element at IF = 7.5 A DC is 1.05 V. We need the VF_bridge per element at an IF = 4.34 A for calculating loss.
Thanks and regards,
Milarepa