Part Number: TIDA-010057
Other Parts Discussed in Thread: TX7332,
Hello, every one,
I use SWAROOP+ TIDA-010057 handheld ultrasound project, when debugging with an oscilloscope can be tested to TX7332 output pulse, while running HSDC ProGUI can not capture data, I do not know why? My steps are as follows;
1. Connect SWAROOP and TIDA-010057;
2. Connecting USB and JTAG;
3. Power on and run the HSDC Pro GUI;
4. Initializing equipment;
5. Set the number of TX and RX channels;
6.pressconfiguresystembutton;
7. Measure the JP1 point of SWAROOP and TX7332HV output pulse with oscilloscope. The measured waveform is shown in the following figures;

8. Click the capture button, as shown in the following figure, but no waveform is read;

9. The voltage of TIDA-010057 is normal;
10. If I replace a piece of TIDA-010057 and run the above 9 steps, the data can be captured, as shown in the following figure;

11. What is the reason for this? How do I find the cause of the defect?
Thank you!
Best wishes!
Chime Xia