This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

waveform generation support on TINA



Hi Team I need support to generate Amplitude shift keying and frequency shift keying waveform on TINA.

Frequncy varies from 100Khz - 400Khz

The waveform can beapproximately described as beginning at the 0° point at 203 kHz and linearly sweep in frequency versus time to a
frequency of 400 kHz in 63 μs (19 full cycles), then linearly sweep to 100 kHz in 4 μs (1 full cycle), and then linearly
sweep to 203 kHz in 33 μs (5 full cycles). The resultant waveform is thus 100 μs ± 100 ns ending at the 0 degree point
after 25 cycles.