Are there any plans to include TPS24700 / TPS2410 controller as a component in Tina simulator.
I have an application where the TPS24xx is on a plugin cards (Dual redundant supply) & the load (5V Logic cpu cards & downstream 35V DC-DC converter cards) is a several meters of cable & significant load capacitance.
It would be nice to simulate this circuit & compare to real world observations.
There is a TPS24700 spice model listed on "Simulation Models released in May 2011", but I think it would take significant effort maybe for me to get this into Tina ?.
Thanks
Toni