Part Number: TIDA-01160
Other Parts Discussed in Thread: UCC21520
Hello all,
I want to use the gate driver power supply used in the TIDA-01160 to power the output of a dual-channel gate driver 'UCC21520' and not a single-channel gate driver like in the reference design.
And in the schematic, the transformer has 2 secondary windings (image below) but when I contacted Wurth Elektronik for the datasheet it turns out it has only one secondary winding.


My questions are:
Is there a similar part number to the 750343468Rev02 with similar characteristics that have 2 similar secondaries I can use in my design?
Or can I use a +15/-8 DC-DC converter module? because it would make the solution cheaper and more compact!
Can the LM25017MRX/Power supply handle a dual-channel gate driver, meaning driving 2 MOSFETs? If not what changes i could make to the power supply to make it work?
Thank you,