Part Number: PMP10200
Other Parts Discussed in Thread: UCC28700,
We have isolated DC-DC power supply requirement as per below data.
Input voltage range 24DC to 500VDC 50Hz & 60Hz
Output voltage +15VDC @ 1.3A, -15VDC @ 200mA
Output wattage requirement (nominal working condition) 20W
I have found a design which is close match to requirement https://www.ti.com/tool/PMP10200?keyMatch=PMP10200. Could you please provide the design calculation as it's not available online?
Also suggest if you find any other design for which EVM board are available.