Other Parts Discussed in Thread: THVD1410, SN74LVC1G123, TRS3232,
Hello,
I'm trying to reproduce the TIDA-060008 circuit but with THT components (and without the optoisolator). I replaced the TRS3232 component by the ICL3232 component, the THVD1410 component by the SN65HVD485 component and the SN74LVC1G123 component by the SN74LV123 component. I reproduced exactly the same schematic (with the same passive component value) as the one in the datasheet TIDA-060008. For my test, I shunt the TX and RX on RS232 side (pin 7 and 8 of the ICL3232 component). When I send on a terminal a letter or other, I do not receive the same character in return. Looking at the oscilloscope, my signal on pin A and B of the SN65HVD485 at the time of sending is not good (see picture). So I disconnected the Q pin of my vibrator. When I tested, with the oscilloscope, my signal was good. Unfortunately I need the vibrator to communicate in both directions, would you have an idea of my problem?