Part Number: PMP11090
Other Parts Discussed in Thread: UCC28700, PMP10397, PMP7668, UCC28722, PMP11302, UCC28881, UCC28710
Hi,
For a project I'm working on, I need to design a 3.3V power source (to power a microcontroller and measure circuit), the max load should be about 100mW. I only have a voltage source around 1000V next to it and I have to use it to make the 3.3V voltage source and since I need this circuit to be as small as possible I want to avoid using a transformer so flyback converter isn't an option. I know converting 1000V to 3.3V in one stage isn't possible since the conversion ratio is enormous so I'm planning to make it in at least 2 steps, I would like my first step to be at around 25V (1/40 reduction ratio).
I struggled to find such high voltage input and low power converter application circuit but I came across the PMP11090 application circuit:

I'm wondering if it would be possible to modify it to make it widthstand 1kVdc entry instead of its actual 440Vac. To do so I would :
- Remove the rectifier part since my input is already DC
- Remove the High voltage pin connection (since it can handle only 700V max input), I would create a start up circuit using a high value resistor connecting the 1000V to VDD as in ucc28700 application circuit (Rstr) :

- Use higher voltage break out mosfet, diodes and an inductor suited for the current spike
I think that by doing these modifications the component should be able to widthstand the 1kV entry but I would appreciate to have second opinions on this. One thing I'm afraid of is the Ton time on the mosfet on the test report of pmp11090, they provide the diode voltage at 440Vac (622Vdc equivalent) and it seems that Ton is about 500ns and it would be even shorter if using 1000Vdc input.

If you have any idea of circuit more suited for my goal, don't hesitate to tell me!
Thanks a lot!