This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Team,
Good day. I am posting this inquiry on behalf of our customer.
This problem occurs when I compile TIDA-010024 {6lowpan stack project}, which is dependent on SDK 2_40_00_81, with a newer version SDK_3_40_00_02.
<Linking>
error: symbol "NOROM_ChipInfo_GetChipType" redeclared with incompatible type:
"ChipType_t()[enum $$fake10933
CHIP_TYPE_Unknown = -1
CHIP_TYPE_CC1310 = 0
CHIP_TYPE_CC1350 = 1
CHIP_TYPE_CC2620 = 2
CHIP_TYPE_CC2630 = 3
CHIP_TYPE_CC2640 = 4
CHIP_TYPE_CC2650 = 5
CHIP_TYPE_CUSTOM_0 = 6
CHIP_TYPE_CUSTOM_1 = 7
CHIP_TYPE_CC2640R2 = 8
CHIP_TYPE_CC2642 = 9
CHIP_TYPE_unused = 10
CHIP_TYPE_CC2652 = 11
CHIP_TYPE_CC1312 = 12
CHIP_TYPE_CC1352 = 13
CHIP_TYPE_CC1352P = 14
CHIP_TYPE_CC2652P = 15]"
in "./../../../driverlib/chipinfo.c" at line 123 and:
"ChipType_t()[enum $$fake10641
CHIP_TYPE_Unknown = -1
CHIP_TYPE_CC1310 = 0
CHIP_TYPE_CC1350 = 1
CHIP_TYPE_CC2620 = 2
CHIP_TYPE_CC2630 = 3
CHIP_TYPE_CC2640 = 4
CHIP_TYPE_CC2650 = 5
CHIP_TYPE_CUSTOM_0 = 6
CHIP_TYPE_CUSTOM_1 = 7
CHIP_TYPE_CC2640R2 = 8
CHIP_TYPE_CC2642 = 9
CHIP_TYPE_unused = 10
CHIP_TYPE_CC2652 = 11
CHIP_TYPE_CC1312 = 12
CHIP_TYPE_CC1352 = 13
CHIP_TYPE_CC1352P = 14]"
in
"C:/.conan/6kvzh_ig/1/source/ti/devices/cc13x2_cc26x2/driverlib/chipinfo.h"
at line 357)
For your information, I am trying to turn on the TCXO. The goal from compiling TIDA-010024 with a newer version of SDK, turning on the TCXO component
Please help to advise. Thank you for extending your support.
Kind regards,
Marvin
Hi Marvin,
TIDA-010024 is not recommended for new designs which means that software is discontinued and not maintained in new SDK versions. As the TIDA-010024 page mention customers should transition to WiSUN which can be found under https://www.ti.com/wireless-connectivity/wi-sun/overview.html
Let me know if you have any further questions.