Part Number: PMP8740
Other Parts Discussed in Thread: UCC28951, UCC28950, MSP430F2252
Hi Team,
Our customer built the PMP8740 using the gerber files from the product. He experienced some issues as discussed below.
We use the BOM of PMP8740 to build two pieces of PCBA.
The PCBA we found problem were listed below:
1.The board output voltage can be adjusted from 24V to 32V is ok. But once we loaded with a few mA current and the voltage drops to zero very quickly. It seemed some kind of protection function was activated. We check
the soldering parts and found no error.
2.The firmware Software Rev_D can support either stand- alone 2KW Power supply or just a charger?
We never designed the UCC28951 chip before.
We use the PM8740 Gerber file to make PCB and according to BOM to buy the parts
But we met another problem was the board is very to explode ;when it loaded with larger current or switch to 24V or 32V .All of 10 pieces of MOSFETs were punch through---Vpfc 390V short to ground.
What could be the issue with the board?
Regards,
Danilo