Other Parts Discussed in Thread: BQ24640, BQ33100
Hello,
I have a questions regarding TIDA-01385 reference design for energy harvesting. This reference design is intended to power a single supercapacitor. I am currently working on an application where multiple super capacitors are to be used to provide power over a longer interval.
Would this design also be applicable here to use multiple capacitors in series instead of one or should a charge controller like the BQ24640 already be used here?
If several supercapacitors are used, it is recommended to monitor them via a charge control. Here I found the BQ33100 super capacitor health manager. Would this be suitable in combination with the reference design?
Many thanks in advance,
Alexander