This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PMP22650: TMS320F28388D

Part Number: PMP22650
Other Parts Discussed in Thread: TMS320F28388D, , TIDM-02013

Hi, Can you tell me if you have used both cores of the a TMS320F28388D microcontroller for PMP22650 project? Thanks

  • Please note that there are 5 cores on the TMS320F28388D device. Only a single C28xCPU is used for the PMP22650 project. This code has since been ported to F28003x which more appropriately fits this application. The F28003x device uses both its C28x CPU and CLA core to run the project. this is because the clock frequency of F28003x is only 120MHz compared to 200MHz on F2838x.

    The F28003x code can be found here: listed as TIDM-02013 https://www.ti.com/tool/C2000WARE-DIGITALPOWER-SDK 

    Regards,
    Cody