When I simulate current of input inductor and output voltage I have big delay, while current and voltage start reise.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
When I simulate current of input inductor and output voltage I have big delay, while current and voltage start reise.
Hi Dorde,
More details are required before we can support you.
Best Regards,
Feng Ji
Hi Feng,
I am simulating a boost converter with an LM5122 control circuit. The current through the inductor should be 60 A,
and the output voltage 15 V.
Input voltage is 3 to 6.8 V, maximum output current is 26 A.
Those signals are not a big problem, I get the values I need.
But for the simulation to start, it takes a very long time of 14ms (it has a big delay).
I am sending a graph with signals, where the inductor current is shown in green, and the output voltage in red.
The capacitor on the Soft Start pin in my case has a value of 360 nF and gives a good result for the signal,
but it has a large delay.
Best regards,
Dorde
Hi Dorde,
thanks for sharing. Will look into that but may needs some days.
But give you some update every 2-3 days.
Best regards,
Stefan
Hi Dorde,
this delay is the startup delay which is due to the charging of the cap at SS to the startup voltage of ~ 300mV.
This delay is required to ensure the boot cap is charged.
See also Datasheet Figure 22
Best regards,
Stefan