Other Parts Discussed in Thread: TPS65987D, , TPS65988, TPS65987
Hello TI -
I'm using a pseudo copy of the TPS65987D based power duo SINK board in our production test fixture. It's intended to negotiate 5, 9 and 15V from our board under test and then we attach a load and verify the current that flows through it. To push the buttons we've successfully connected the device to SPI port expanders and our board under test drives those fine. I am having trouble with the controller itself though and I was wondering if you can send me a copy of the parent project for generating the image that gets loaded onto the power duo board... I'm specifically interested in the VBUS powered or lower half of the reference board which i thin kis TIDA-050014... I am specifically looking for all of the contract and GPIO settings that are used so that i can set up our tester board's TPS65987D image.
Thanks very much,
Adam