Part Number: TIDA-010062
Hi Champ,
I am asking for my customer.
In ttppfc stage in F28003x, designer calls the function ADC_setPPBCalibrationOffset to set up PPB offset calibration for ADCA module.
(1). What is the main purpose to call the function ADC_setPPBCalibrationOffset at here in application ?
(2). Continue to (1)., is it a must need to call the function ? If yes, on the customer's board, how to make adjustments for the offset value ?
(3). Continue to (1). how about ADCB and ADCC module ? Why aren't these two ADC modules been calibrated ? Do we need additionally put code to calibrate ADCB and ADCC offset ?
Thanks and regards,
Johnny