This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Need additional information regarding LMG3526R030

Other Parts Discussed in Thread: LMG3526R030, LMG3522R030

Hello,

Could you please send me the PSPICE model for  LMG3526R030. Also the data sheet for the same does not mention about the Eon and Eoff (Energy) for the switch. Could you also provide me that information.

Thanks,

Neha Agarwal.

  • Hi Neha,

    We don't currently have a PSpice model for the LMG3526R030, however the PSpice model for the LMG3522R030  will be the same as it will be for the LMG3526R030 device with the exception of the /OC -> ZVD pin. On the LMG3522R030 the /OC pin reports out over current faults in tandem with the /FAULT pin. On the LMG3526R030 the pin is the ZVD pin and reports out when zero voltage switching has occurred.

    This part is newly released and we are still working on collecting this data. In the meantime, please refer to Eon & Eoff plots in the LMG3422R030 data sheet. These numbers will be similar between the two devices.

    Best,

    Kyle Wolf

  • Thank you so much.