Part Number: TIDA-010085
I would like to know how the 'C' wire is connected in the TIDA-010085 reference design. Is the ISO_GND connected to the 'C' line in the HVAC system?

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TIDA-010085
I would like to know how the 'C' wire is connected in the TIDA-010085 reference design. Is the ISO_GND connected to the 'C' line in the HVAC system?

Hi Adnan,
For this design, the ISO-GND is not connected to the C wire, but is a floating ground (part of the isolation rail for the gate driver for each SSR). The C wire will come from the 120V->24VAC transformer and is a common connection to each SSR, and can be used for powering remaining portions of the SR board.
-Brian