When I run circuit #1 (see image), PSPICE works great.
When I run circuit #2, which is circuit #2 doubled (in parallel), I get errors.
Does PSPICE allow running two identical circuits from the same Source?
If YES, how would I configure circuit #2 for proper simulation?
Here's the error message: ERROR(ORPSIM-15143): Voltage source and/or inductor loop involving X_U4.X_H1.VH_H1. You may break the loop by adding a series resistance.
(adding series resistance to the Source output doesn't change the error)
CIRCUIT #1 (works)

CIRCUIT #2 (error)