This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PMP11371: UCC28740DR

Part Number: PMP11371

i  am working on 5.5V/11Amp fly-back power supply. the circuit and reference design i took from the Texas Instruments website which reference number is (PMP11371) i took same same components same design and same IC  technique for my design. i dont have the transformer design and data but with the help of google and few notes on Fly-back transformer design  i made and circuit is working properly without any problem. but problem is this i am not getting my desired output. my design is providing me only 5.5V/10amp supply. previous mail i told you my transformer design data. which i am using with the reference design. please help  me to find out the  problem where i am  doing mistake.
 As per your knowledge i am sharing the link of my reference design, the reference design number. and transformer design data.
 
Transformer Design Data is.
Winding
Start
Finish
Turn 
Wire gauge and wire number
Primary Winding 1
3
27
0.4mm*3
Secondary Winding
9/10
11/12
3
650*0.07mm litz wire
Aux Winding
6
5
5
0.5
CORE-PQ2625
 
  • i  want to run my device on minimum 90 DC volt to maximum 375 Dc volt. recently my device is working on minimum 120DC volt. my requirement are minimum Dc 90V and maximum Dc 375 V. and output 5Vdc and 12 amp current. which components should i change. please help me to find out this .