I am simulating the step response waveform of an RLC circuit with TINA. Input a step signal and examine the voltage waveform across the capacitor. Setting R = 0Ω, L = 1µH, and C = 1µF, the result obtained by Analysis > Transient Analysis > should be that the vibration should continue, but the vibration waveform converges to an amplitude of 1. I don't think there is an error in the settings, but if there are any inadequacies, it would be helpful if you could point them out.