This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PMP40801: Is there a way to make the PMP40801.4 to also have a sink function

Part Number: PMP40801
Other Parts Discussed in Thread: TPS65987

Good afternoon,

I was wondering if it were possible to  see the schematic of the PMP40801.4. I was also wondering if it were possible to use the GUI to operate this design to act like a sink as well as output at least 65W.

Thank you,