Part Number: TIDA-010025
Other Parts Discussed in Thread: UCC23514, SN74ACT244
Hi,
I hope my email finds you well.
I am a UT Dallas student. I read the reference design TIDA-010025 (Three-phase inverter reference design for 200–480 VAC drives with opto-emulated input gate drivers). I have some questions about the gate driver part of inverter.
1. In the Figure 3. in reference design, it stated that x4 (+15V and -8V) isolated power supply have been used. It means three +15V and one -8V have been used or four +15V and four -8V power supply is needed?
2. In Figure 9. in reference design, for high side IGBTs definitions (VCC-U and VEE-U) and for low side IGBTs (VCC and VEE) have been used. Can you please tell whether their value or sign (+ and -) are different or they are the same? I mean for both high and low side IGBTs these value are the same or should be different?
Many thanks for your consideration and supportive guidance as always.