Part Number: TIDA-01599
Other Parts Discussed in Thread: ISO1211
Hello,
Does the STO inputs from J5, 24V* And can you share the output value of the iso1211dr ? I'm designing and STO board and I have 2 external inputs for 24V STO signals and I need to use them on a safe MCU which has 3.3 V input so I was wondering if I can use the same method as TIDA and if ISO1211dr is suitable for it?
Thank You & Best Regards