Other Parts Discussed in Thread: THS4531, , ADS8354, THS4531A
Hi Team,
Good day. I am posting this inquiry on behalf of the customer.
I would like to take over the reference design TIDA-00178 for a project. In the example project, a gain factor of 5 is set for the THS4531.
As a power supply, the chip has 5 V. If I amplify 1Vpp by 5, then I have between 0 and 5V. The output voltages do not go up to 5 V, but rather 4.9 V.
If my 5V power supply fluctuates by 5%, it gets even less.
So with a gain of 5, I will have problems in the 0V and 5V limits.
The signal is cut off above and below.
What am I missing here? I'd love it if you could help me.
Thank you for extending your support. Your help is much appreciated.
Kind regards,
Marvin