This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PMP11612: Solution 1A AC to DC Power Supply

Part Number: PMP11612
Other Parts Discussed in Thread: UCC28704

Hi,

I am designing AC to DC SMPS in automation Field. My Power Supply is requirement in below details-

  1. Input Voltage - (85 to 264) VAC 
  2. Output Voltage- 5VDC/1A or 5VDC/2A (Both are given)
  3. Voltage Accuracy- 1% to 2%
  4. Power -5W/10W
  5. Line and Load Regulation- 2%
  6. Ripple- 50 to 150mV
  7. Efficiency-80 to 90%
  8. Isolation- 4000VAC (Input to Output)
  9. Protection- Over Current, Short Circuit, Over voltage and Temperature Protection.

I have searched some solution. I have some query as per below Reference Design-

Reference Design Number- PMP11612 (85-265) VAC

  1. Can This Power Supply working input  Voltage (75 to 275)VAC

Lower Voltage -75VAC and Upper Voltage-275 with 5V/1A and 5V/2A

  1. I want to set output Voltage 5.1 or 5.2VDC. Which resistance value is change in Circuit?
  2. I want to set input under voltage and input over voltage limit. How will be set in circuit.
  3. If Load variation(200mA,500mA,1A,2A) output voltage is constant
  4. Line variation-? Load variation-?
  5. I seen part number of transformer 10339-T048 in BOM but there is no stock. Please suggest me any alternate part number of transformer.
  6. What is size of PCB and BOM Cost.