This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TIDA-020047: PMIC LP876242B0RQKRQ1 have no output.

Part Number: TIDA-020047

Dears

  We use TIDA-020047 reference design to make board, and its design and Bom are adopted the reference design without any changes. PMIC LP876242B0RQKRQ1 have no output both four buck after power on. SW pin has no output, Vout_LDO output 1.8V, how to solve this problem? Do you need to configure the GPIO pin? The SOC is not powered on, and registers cannot be configured.