This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SwitcherPro wrong model parameter(s)?

Dear Community,

i wanted to use the Renesas RJK0305DPB MOSFET in a design, but

the parameters that are stored in SwitcherPro are not the same as i found in the datasheet.

The Current e.g. is mentioned with 15A instead of 30A (abs. Max) in the datasheet.

Gate Charge is mentioned with 70nc. In the datasheet Total Gate Charge Tg is mentioned with 8 nC?

Do i interprete the datasheet wrong?

 

Regards

Christoph

 

 

rej03g1353_rjk0305dpbds(1).pdf
  • Hi Christoph,

    You are right. We have wrong values for MosFET in our library. We will correct it in our next version releasing on 8/31.

    Thank you for reporting this and helping us improve the quality of our software.

     

    Thanks,

    Hetal Joshi

    Senior Developer and Project Manager

    Analog eLab Design Center

    HPA Design Tools

    Texas Instruments, Inc.