This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TIDA-00874: What is the purpose of 10kOhm and 22pF between input and output? Why are they not placed?

Part Number: TIDA-00874
Other Parts Discussed in Thread: TPA3251

In the schematic file we can see four groups of RC connected between input of TPA3251 and output. What are the purpose of these components? Why are they not placed?